4/14/2016 12:45 AM | |
Posts: 11 Rating: (0) |
Good afternoon. Dear friends, I am integrating SIPROTEC compact IED IEC -61850 sicam network in a V6, but I have problems with the upgrade module OPERATION,. The import of network interface .scd file to IEC61850, was successful in the Configuration module, but when we will monitor the variables in the Value Viewer are not available, the system update on Operation was performed but the IED, does not connect. The question is, version 6 Sicam compatible with 7SJ80xx or 7SK80xx reles,. Additionally someone could help us with some way to solve and to communicate this FDI. Thanks in advance for your help .. Attachment1.docx (80 Downloads) |
4/15/2016 2:48 PM | |
Posts: 11 Rating: (0) |
Yes, Mike. In DIGSI the IEC network upgrade was done, export the project to date and subsequent import to sicam it became, as seen in the prt.sc. Let you know that this communication architecture according to the attached document, it is possible that the fault is in the RS900 switch that are not configured in the domain of network sicam? The switch 2100 is as a device within the sicam settings and RS900 are not listed ..... This think is the problem ... ???? Thanks Mike for the support.
AttachmentArq.docx (76 Downloads) |
4/26/2016 11:12 PM | |
Posts: 11 Rating: (0) |
Hi Mike. Sorry for the response time. Sicampas confirmed that the V6 is running on the Windows XP operating system. Orange boxes are fiber optic patch cord to carry 250 mts communication between 2 switch RS900. Likewise I confirm that the test via ping from the switches to the sicam respond normally. I will be attentive to your answer. Attachment sending the updated architecture. Best regards.
AttachmentArq.docx (56 Downloads) |
5/5/2016 3:47 PM | |
Posts: 11 Rating: (0) |
Hi Mike... Let you know that after much work we finally managed to establish communication with IEDs according to the following description. 1. We had to make the configuration of the RS900 Switchs within the project and include sicam SU network. 2. Following this suvimos firmware to the relays 7SJ80x 7SK80x to v4.73 and v4.74 for new relays. For a project that originally had the 7SJ80x firmware v4.64 and v4.64 7SK80x can not enter into the IEC network. The IECbrowse can not communicate, auque IEDs are inside the network (ping). The new project sicam agree to the attached document ... Now we have to change the draft relays that are developed with device driver update 4.64 to 4.73 and 4.74 respectively in the DIGSI v4.88 ..... What we could not make it up in a direct way the firmware 4.64 to 4.74 in the 7SK80x teams we have to go first to load a project 4.72 and later firmware update to 4.74 and finally initialize the new configuration relay with 4.74. You aware if there is any alternative procedure. I appreciate your cooperation we are attentive to your answer.
Attachmentconfiguration of the sicam.pdf (103 Downloads) |
Last edited by: Min_Moderator at: 5/9/2016 1:59:03 PMConvert attachment to pdf |
|
Follow us on