5/5/2020 9:47 PM | |
Joined: 12/18/2014 Last visit: 12/1/2023 Posts: 31530 Rating:
|
The LOGO! has no function block to convert from HEX to decimal. You must program the converting by your self. |
5/5/2020 10:37 PM | |
Joined: 2/22/2008 Last visit: 11/30/2023 Posts: 2698 Rating:
|
Do you mean Hex or BCD format ? Have you a link to your device ? I have some converter in the german forum, here is the Link to converter Regards, Scorp |
5/6/2020 9:34 AM | |
Posts: 40 Rating:
|
Example from the manual:
|
5/6/2020 9:56 AM | |
Joined: 2/22/2008 Last visit: 11/30/2023 Posts: 2698 Rating:
|
Ignore this text, this is only a number representation, you can write 16x0F or decimal 15, the bits are the same..Try out the program in attachment in a simulation. Copy this part into your programm with ready network setup and change the analog network input to your proper value. Regards, Scorp AttachmentTemp1.zip (103 Downloads) |
This contribution was helpful to
1 thankful Users |
5/6/2020 11:40 AM | |
Posts: 40 Rating:
|
Thank you, Scorp Simulation just works, so now I can probably order the device I mentioned with some level of confidence. |
Follow us on