2/8/2016 9:02 PM | |
Joined: 12/27/2006 Last visit: 7/7/2024 Posts: 1197 Rating:
|
Not all the LOGO! types have High-speed inputs. What LOGO! do you have? |
2/8/2016 9:14 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
In my opinion it is the voltage level. According to the manual, the voltage level <5V as 0 signal is defined. The voltage level> 8.5 V is recognized as a 1-signal. The problem will be not working your pulse generator with the necessary voltage level in order to ensure a clear Count. AttachmentLOGO! Soft manual 0BA6 03_2009 side 253.pdf (157 Downloads) |
This contribution was helpful to
1 thankful Users |
2/9/2016 4:33 PM | |
Posts: 158 Rating:
|
got it running on a 12V battery now, working ok, input 6V pulses instead of 4V..... |
2/9/2016 7:42 PM | |
Posts: 158 Rating:
|
well over 12,000 cycles now...pretty sure it was low voltage. |
2/9/2016 8:18 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
You're in luck. Actually, the voltage level is still too low with 6 VDC. |
Follow us on