Industry Online Support
Technical Forum
3/11/2013 3:25 PM | |
Posts: 2930 Rating: (432)
|
Hello, No, you LOGO! doesn't have high speed inputs. High speed inputs are only available at DC Version of LOGO!. Hope this helps |
3/12/2013 1:30 PM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715)
|
Hello, You need highspeed inputs, that leaves the LOGO! 24C, 8DI(4AI)/4DO, 200 BLOCKS and With first one you need external relais to control 230V outputs, with 2nd one the buildin relais can handle loads (resistive) up to 10 A. My advice is always use external relais to switch that kind of load, easyr to replace if relais is broken. If you need more than 200 blocks then go for the OBA7 range. http://support.automation.siemens.com/WW/view/en/50440013 regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
3/12/2013 11:22 PM | |
Posts: 3 Rating: (0) |
Thanks Marcjan, 12/24rc on order. |
Follow us on