2/9/2021 2:10 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello It important to know which HMI Device do you want to use? IF you have a Comfort Panel or a Advanced Runtime (PC Based Runtime) Then you can use the Scheduled Task to run a Script twice a Day as you needed and write the Value and information you want in a CSV File: https://support.industry.siemens.com/cs/ww/en/view/59604194 https://support.industry.siemens.com/cs/ww/en/view/106501825 If you use a Basic Panel then you cannot do scripting. here you only can use the Process Archives. Here you can use Log on Demand and also the Scheduled task to run the LogTag Systemfunction. But you should use also time Synchronisation here. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
2/10/2021 5:14 AM | |
Joined: 9/9/2015 Last visit: 10/19/2022 Posts: 22 Rating:
|
Thank you for the helpful information! Best regards! |
Last edited by: Klepa at: 02/10/2021 05:16:11 |
|
Follow us on