1/23/2012 8:42 AM | |
Posts: 7 Rating:
|
hi , read this .
Attachmentutilisation de winpcin.pdf (327 Downloads) |
1/26/2012 7:35 AM | |
Posts: 288 Rating:
|
hi which file is wincc flexible file which i should transfer to my pc(with winpcin) to be able to open it? best regards. |
1/27/2012 6:37 PM | |
Posts: 2964 Rating:
|
Hello... Software requirements Requirement: The software below is required prior to installation of SINUMERIK HMI WinCC flexible configuration software: For SINUMERIK HMI devices ● WinCC flexible 2007 ● For HMI-integrated work, a SINUMERIK HMI Advanced 7.1 or 7.2 SP2 or 7.3 For SIMATIC CE Panels ● WinCC flexible 2007 The SIMATIC packages are not part of the SINUMERIK HMI WinCC flexible configuration software. Check this PDF for the details. http://support.automation.siemens.com/WW/view/en/28737264 Regards, Prakash |
This contribution was helpful to
1 thankful Users |
Follow us on