6/2/2013 8:38 PM | |
Posts: 8 Rating:
|
Hi I configured a new alarm class with status texts: Incoming: Activated Outgoing: Deactivated For incoming signal I get alarm status: Activated But for outgoing: ActivatedDeactivated For outgoing signals I would like to see status: Deactivated.
|
6/3/2013 2:36 PM | |
Posts: 3037 Rating:
|
Hello matiop, Your project works fine. The alarm system works so. If the alarm is coming, you see " Activated" if the alarm is going out, you see "ActivatedDeactivated" If you use an alarm with acknowledgment. Then you see: If the alarm is coming, you see " Activated" if the alarm is going out, you see "Activated Acknowledge" if the alarm is going out, you see "Activated AcknowledgeDeactivated" Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on