11/13/2013 6:58 PM | |
Posts: 40 Rating:
|
Hello, it's my first test with HMI programming. I have a S7 1200 and i want simulate a HMI. I have some problems about the connection between HMI and PLC. I wanna simply show a an external variable that i have put in the HMI. The error message says "Connection HMI - the local subnet and that of the patner are different" How can i solve it? Thanks a lot AttachmentDocumento1.pdf (318 Downloads) |
11/14/2013 3:52 PM | |
Posts: 40 Rating:
|
Now i have used a ethernet interface but i have troubles about yet. Where is my fault? Thanks AttachmentDocumento1.pdf (300 Downloads) |
11/14/2013 3:58 PM | |
Posts: 1299 Rating:
|
Hello, you have to connect the hmi with the plc. K!ke |
11/14/2013 4:59 PM | |
Posts: 40 Rating:
|
Ok, i've done. Why now do i see "########" in the I/0 label? Thank you very much Attachmentx.pdf (307 Downloads) |
11/18/2013 5:18 PM | |
Posts: 1299 Rating:
|
Hello, do you have a physical connection between the pc with the simulationand the plc? whatdid youset in PG/PC-interface in control panel of the pc? K!ke |
11/18/2013 6:23 PM | |
Posts: 40 Rating:
|
Yes, i have a physical connection between pc and plc. How can i connect virtually the HMI? AttachmentDocumento1.pdf (381 Downloads) |
11/19/2013 4:51 PM | |
Posts: 1299 Rating:
|
Hello, you have to start simulation to access the hmi K!ke |
Follow us on