4/11/2019 6:57 PM | |
Posts: 45 Rating:
|
How do I make one button on the HMI turn on an output on the PLC and a second button on the HMI turn it off ? |
4/11/2019 9:36 PM | |
Posts: 45 Rating:
|
Are you guys telling me that a setbit command in the HMI can change an output on the PLC if the tags are configured correctly ? |
4/12/2019 10:59 AM | |
Posts: 2826 Rating:
|
Hello. Please find attached a demonstration project for TIA V15 containing a PLC program and HMI program, which I designed for you. Four (documented) methods are demonstrated to switch outputs. It includes memory usage tips and use of "animations" (colour changes). The ZIP attachment contains a helper picture and a ZAP15 archived project. Feedback is welcome. Attachmentdemonstartion.zip (216 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on