4/11/2019 6:57 PM | |
Posts: 45 Rating: (0) |
How do I make one button on the HMI turn on an output on the PLC and a second button on the HMI turn it off ? |
4/11/2019 9:36 PM | |
Posts: 45 Rating: (0) |
Are you guys telling me that a setbit command in the HMI can change an output on the PLC if the tags are configured correctly ? |
4/12/2019 10:59 AM | |
Posts: 2826 Rating: (684) |
Hello. Please find attached a demonstration project for TIA V15 containing a PLC program and HMI program, which I designed for you. Four (documented) methods are demonstrated to switch outputs. It includes memory usage tips and use of "animations" (colour changes). The ZIP attachment contains a helper picture and a ZAP15 archived project. Feedback is welcome. Attachmentdemonstartion.zip (143 Downloads) |
This contribution was helpful to2 thankful Users |
4/12/2019 8:48 PM | |
Posts: 45 Rating: (0) |
With screen shots of the code and the tag tables I could type the program into my TIA V12 and be able to run it. |
4/12/2019 10:40 PM | |
Posts: 2826 Rating: (684) |
Reply 1 of 3: Project as PDF files. Attachmentproject-as-PDF.zip (110 Downloads) |
Last edited by: #dP at: 4/12/2019 10:50:11 PM3 messages .. memory allowance is too small |
|
This contribution was helpful to1 thankful Users |
4/12/2019 10:48 PM | |
Posts: 2826 Rating: (684) |
Reply 2 of 3: (PLC) Project as screen captures (PART1). Only important sections highlighted. Notes included. Attachmentproject-as-pictures-with-notes-PART1.zip (111 Downloads) |
This contribution was helpful to1 thankful Users |
4/12/2019 10:49 PM | |
Posts: 2826 Rating: (684) |
Reply 3 of 3: (HMI) Project as screen captures (PART2). Only important sections highlighted. Notes included. Attachmentproject-as-pictures-with-notes-PART2.zip (101 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on