10/5/2021 1:23 PM | |
Joined: 5/31/2021 Last visit: 4/6/2023 Posts: 1 Rating:
|
Hey experts, I am working with 1510sp-1 PN cpu and KTP 700 basic HMI , in the middle there is a ethernet switch . so I can able to download the program to cpu and the design to HMI as an individual. but the problem is that the HMI doesn't fetch data from plc. plc is ok it send the data in vfd as well. after downloading whenever I start the HMI a "connection disconnected" alarm pop up will appear. when i troubleshoot about it I found that the HMI connection done in the network is fine ,and also there is no issue in the port. but still I am facing that issue. can you guys please help me to come out from this issue ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2021 09:10:35New subject after splitting |
|
10/14/2021 2:09 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello Check your configuration, perhaps it leads to the reason: https://support.industry.siemens.com/cs/de/en/view/89852595 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on