1/14/2014 5:16 PM | |
Joined: 10/1/2013 Last visit: 3/18/2025 Posts: 605 Rating:
|
Hi, |
1/18/2014 7:36 AM | |
Joined: 4/14/2010 Last visit: 2/8/2025 Posts: 525 Rating:
|
Greeting, No, how can change PB profile is it Node address..??? Thanks. |
MS |
|
1/21/2014 11:14 AM | |
Joined: 3/20/2013 Last visit: 3/18/2025 Posts: 676 Rating:
|
so you resolved your problem with a workaround? |
Best Regards, |
|
1/21/2014 3:37 PM | |
Joined: 4/14/2010 Last visit: 2/8/2025 Posts: 525 Rating:
|
Greeting, No, in this way we have to interchange the MPI cable every time for download in both devices CPU or HMI. but interface cable should plug in the CPU MPI port only one time and download the program in both devices CPU and HMI via MPI without interchange the cable. see attched network topolgy and following settings. hmi connected on MPI/DP port slot 7X1 Subnet Profibus_1 type of PG_PC interface = CP5512 PG_PC interface = MPI address for HMI = 4 Thanks. AttachmentDesktop.zip (95 Downloads) |
MS |
|
Follow us on