2/3/2025 2:07 PM | |
Joined: 2/3/2025 Last visit: 2/12/2025 Posts: 2 Rating:
|
HI, our HMI (TP 700 Comfort ) showing Alarm Application Error (Application Scs Server.exe encountered a serious error and must shut down ) After that we Power ON-OFF the HMI, but HMI Not getting ON. Please support. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/03/2025 14:34:36New subject after splitting Last edited by: AutoGen_5952102 at: 02/04/2025 07:50:42 |
|
2/3/2025 3:08 PM | |
Joined: 7/11/2024 Last visit: 4/16/2025 Posts: 185 Rating:
|
Hello, Which panel are you using? Have you tried updating the firmware version of the panel? You can find the files in the next FAQ:Image Downloads for HMI Operator Panels Also, you should delete the IM folder of the project to avoid inconsistent contents. Follow this FAQ: How do I delete the IM folder of my TIA Portal project? Good luck! |
If this post has been useful, don't forget to rate it!😊 |
|
2/4/2025 3:53 PM | |
Joined: 7/11/2024 Last visit: 4/16/2025 Posts: 185 Rating:
|
Hi If the firmware update does not solve the problem, you should try a factory reset via Prosave. Take a look at this: How do you do a SIMATIC HMI operating system update (firmware update, OS update) on operator panels or perform a "Reset to factory settings"? |
If this post has been useful, don't forget to rate it!😊 |
|
Follow us on