9/26/2016 7:26 AM | |
Joined: 2/27/2014 Last visit: 2/5/2025 Posts: 689 Rating:
|
Hello, Yes, its possible with script supported panel also and non script supported panel. See the below application to fulfill your requirement. Connecting SIMATIC HMI Panels with SIMATIC S7-400H (WinCC V13 and STEP 7 V5.5)https://support.industry.siemens.com/cs/us/en/view/96837136 You need to use the change connection event in Basic Panel. see the attached pdf file also. If you stuck somewhere then contact me. If you feel this post is useful then don't forget to rate. Attachment96837136_Panels_and_S7-400H_en.pdf (144 Downloads) |
With Best Regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on