9/30/2020 7:10 PM | |
Posts: 25 Rating:
|
Hi Every one I am facing a problem in a system hoping someone can help me. As attached file Our system consist of two redundant CPU S7-412 H, 2 SCALANCE XC206-2 Switches (6GK5206-2BB00-2AC2) and one HMI TP 1500 Comfort, The system connect to DCS through 2 redundant fiber optic cable. The redundant of CPU work very good no problem happened. The redundant of HMI was working ok but after connect the DCS fiber optic cables to the switches the HMI become slow in show Feed back and receive order because I notice that the HMI become Change connection to PLC1 to PLC2 and reverse alone without any problem in connection almost every one minute, also the DCS System Engineer inform us that our system make conflict at DCS system. So now we removed one ethernet cable of two cables connected to HMI then no problem in HMI (slow in Feed back) and no conflict at DCS system but now the HMI connect to CPU1 only. I follow all instruction from Siemens support in this link for establish HMI redundancy https://support.industry.siemens.com/cs/document/96837136/connecting-simatic-hmi-panels-with-a-simatic-s7-400h-(wincc-v16-and-step-7-v5-6)?dti=0&lc=en-ZM and As I mentioned before it was working very good but all problem happen after connect DCS. Ethernet cable was connect to HMI as per attached photo X1 (P1 & P2). Some one suggest to activate Media redundancy for HMI Port but it show me that I have to use it as client an If I select Clint it show me error ( a manger must be configured ). I tried to put all details in attached file as possible. Thanks in advance. AttachmentSystem.zip (166 Downloads) |
10/6/2020 9:03 AM | |
Joined: 5/11/2017 Last visit: 2/4/2024 Posts: 59 Rating:
|
Can you share your current system architecture |
10/8/2020 5:28 AM | |
Posts: 25 Rating:
|
It is already attached with the topic
|
Follow us on