10/10/2022 11:24 AM | |
Joined: 8/3/2009 Last visit: 4/29/2025 Posts: 15388 Rating:
|
Hello BroStaw It looks like you do not have installed the WinCC Panel Images DvD and the Updates to this installation. So the system has the Update for engineering installed and want to use the latest Update Image but its not installed. Should look like-> See attachment So install First the DVD 3 with the Panel images and then the Update package of this FAQ: https://support.industry.siemens.com/cs/de/en/view/109746530 Bye Murof |
Last edited by: Murof at: 10/10/2022 11:26:03Last edited by: Jen_Moderator at: 10/11/2022 07:11:57Text formatting optimized. If this Information really helps, you could use the Rate function |
|
Follow us on