6/1/2012 8:43 AM | |
Joined: 4/22/2010 Last visit: 1/15/2025 Posts: 5697 Rating:
|
Hello That is one off the standard screens, are you sure there is a configuration downloaded to the panel? You can walk trough the other screens with the softkeys. See attached manual for more details. Regards, Marcjan AttachmentOp3_e.pdf (273 Downloads) |
Problem solved? |
|
6/5/2012 3:43 PM | |
Posts: 3037 Rating:
|
Hello, Can you post a screenshot of the error message? Tweety |
1/10/2014 8:21 PM | |
Joined: 4/22/2010 Last visit: 1/15/2025 Posts: 5697 Rating:
|
Hello, That is a message from the panel, not triggered from PLC, try to do a selftest to see what's wrong. See manual i posted in 2nd post Click Chapter 16 in part 4. Maybe the panel lost the configuration, if you have a backup you can try to restore it. If no backup, better stop trying to repair this panel and get a more 2014 model. This is a text based panel and it's not verry hard to program the functions in a new panel. Regards, Marcjan |
Problem solved? |
|
Follow us on