2/7/2024 2:07 PM | |
Joined: 6/30/2023 Last visit: 2/8/2024 Posts: 18 Rating: (0) |
Hello everyone as in the topic How to fix it ? |
2/7/2024 3:15 PM | |
Joined: 5/6/2022 Last visit: 5/16/2024 Posts: 420 Rating: (83) |
Hi WiktorRoz, This error occurs because the simulation has to be downloaded and installed separately (https://support.industry.siemens.com/cs/ww/en/view/109814516), after the WinCC Unified ES installation. The no installation of the runtime package together with old TIA versions can lead to the following error message when trying to start the simulation: "An incorrect runtime version is installed. The installed runtime cannot process the project. Install the runtime manually on the target device ". So check your installed software. And install TIA Portal PC RT V18 and also the latest update: https://support.industry.siemens.com/cs/ww/en/view/109807123 Also check the configuration and the version of your WinCC Unified device in TIA Portal and use the suitable PC Runtime version. Then it should be possible to use the simulation in your project. You can also see the entry in this forum that may be of help, which summarizes a bit of what I'm telling you: "TIP – simulator installation for WinCC Unified V18" Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |