3/4/2020 4:09 AM | |
Joined: 3/30/2014 Last visit: 1/16/2025 Posts: 99 Rating:
|
What functions can this button be used for? |
3/5/2020 9:37 AM | |
Joined: 11/14/2018 Last visit: 4/3/2025 Posts: 502 Rating:
|
Hello o0yuming0o, in general (and technically) you can attach every function you want to the buttons ;) But I think you wanted to ask something like "why there are buttons next to these parameter value outputs and how are they used in regard to the specific parameter?" If you just want to display the value of the parameter, you don't need the button. You can delete it. If you want to be able to change the value from your HMI, you can use the button to open up a pop-up or window. This window then must have a input field and buttons to confirm the change. Regarding HMI design in general, have a look at the "HMI Design Masterclass", I think it's free: https://new.siemens.com/global/en/products/automation/simatic-hmi/design-masterclass.html Bye, |
If I could help you, be so kind and rate my contribution. :) |
|
3/12/2020 9:50 AM | |
Joined: 8/3/2009 Last visit: 4/23/2025 Posts: 15322 Rating:
|
Hello https://support.industry.siemens.com/cs/de/en/view/91174767 Chapter 2.2.2 -> There is a short description of the ideas behind the examples you have mentioned. and of course just have a look in the programming of the project then you can see what it sould do. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on