11/16/2022 1:32 PM | |
Joined: 1/29/2018 Last visit: 1/4/2024 Posts: 10 Rating:
|
Hi guys. I have the also problem with HMITemplateSuite from Library. When creating HMI screen on TP900 all fields look nice and fit to screen. When doing simulation with WinCC RT Advanced fields are cutted and resized and not OK. As a example Text filed are cutted even in set "fit object to content" that do not make sense. Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/17/2022 06:08:49New subject after splitting |
|
11/17/2022 6:11 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
Closed cause question posted twice. The second thread with the subject Change resolution to simulate TP900 with WinCC RT Advanced is published within the conference SIMATIC WinCC (TIA Portal). Jen_Moderator |
This contribution was helpful to
1 thankful Users |
Follow us on