Industry Online Support
Technical Forum
7/16/2008 8:49 AM | |
Posts: 2 Rating:
|
When I try to start WinCC flex 2007 (HF4) I got the following message. "HmiSmartStart.exe has encountered a problem and need to close" What to do? |
7/16/2008 10:33 AM | |
Joined: 5/8/2006 Last visit: 2/22/2023 Posts: 1085 Rating:
|
Hi, maybe this FAQ will help you: http://support.automation.siemens.com/WW/view/de/28465761 Bye |
7/16/2008 2:03 PM | |
Posts: 2 Rating:
|
I deleted Wicc and run the Ceanup tool. Then I made a new installation and got the same problem. |
7/15/2010 6:17 PM | |
Posts: 1 Rating:
|
Sorry this post is a little late, but it may help someone else out. I found out that I had problems with Microsoft .NET Framework. Instead of reformatting your whole computer, I would try to uninstall all of the .NET Framework installations from your machine and then re-install them. BEFORE UNINSTALLING: Note down all versions of .NET Framework that you have installed and use option 2 on to this webpage:http://support.microsoft.com/kb/923100(nice automated removal). When you finish, go back to the same page and download all .NET Framework files you need to reinstall. Don't worry about downloading service packs though - let windows update get you back up to speed. Hope this helps someone!
|
Follow us on