7/17/2017 2:58 PM | |
Joined: 7/19/2007 Last visit: 3/4/2024 Posts: 33 Rating:
|
Hi,
How can a second IP (with a different subnet) be added to the networkcard ? I looked in the network card properties (V13 SP1, upd 9) but the 'change settings' button is disabled (greyed out). I'am logged in as administrator and started Tia by right clicking 'run as administrator'. My IP configuration is fixed (not DHCP). (Why is a second IP necessary when a router is configured between the two subnets ?) Searching accessible devices only shows PLC's in the current subnet. Normal and Extended download failed to make a connection to the IP in the other subnet. Ping to that IP-address answers just fine Are there other ports except for TCP 102 that should be kept open by firewalls ? Thanks for a reply. Kurt ------------------------------------------------------------------------------------------ |
Last edited by: Kurt Pidpa at: 7/17/2017 3:06:02 PMLast edited by: Jen_Moderator at: 7/19/2017 11:25:41 AMNew subject after splitting |
|
7/17/2017 3:45 PM | |
Joined: 5/12/2006 Last visit: 3/21/2025 Posts: 22596 Rating:
|
add the IP in the Windows settings of the Network Card, not in TIA. |
Follow us on