2/4/2008 1:11 PM | |
Posts: 6 Rating: (0) |
Dear bunglehead, I tried to put a bitI0.0 to start a motor from wincc-flexible. If I have CPU in STOP position andI set from wincc-flex I0.0 in PLCSIM the specified input is enable.When I put CPU in RUN position all the value from PLCSIM areremoved If I have CPU in RUN position and I try to set from wincc-flex this I0.0 nothing is changing on PLCSIM. If repeat with CPU inSTOP position I can set this I0.0 I don't any information about this from wincc-flex(not errors show up). Could please tell me what configuration you are using to simulate a project. (what version of S7 you have; What version of PLCSIM; What version of wincc;wincc-fle;protool). Tanks for yourtime. Regards |
2/5/2008 8:28 PM | |
Posts: 54 Rating: (3) |
Try this for settings http://support.automation.siemens.com/WW/view/en/13283804..And this for screenshots (its in russian, but pictures are understandable I hope) http://www.automation-drives.ru/forum/viewtopic.php?t=5222&highlight=plcsim |
2/7/2008 10:47 AM | |
Posts: 121 Rating: (16) |
Best wishes are done with post rating in this forum . I'd could use some. But good that it works now |
Follow us on