11/23/2017 1:42 PM | |
Posts: 648 Rating:
|
Motivation / Benefit Change grafics dynamically while WinCC Runtime is running. Tested with
Add. Information: can be used with higher Versions too Describition To realize the dynamic change of graphics the control HTML browser will be used. The system function “OpenFilebrowser” will show dialog which makes it easy to select the next listed graphic.
Note The shown graphics are scaled to the size of the HTML browser control. Related links Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder. AttachmentScreenshots_English.zip (60 Downloads) |
Last edited by: rh1990 at: 11/23/2017 1:43:02 PMLast edited by: rh1990 at: 11/23/2017 1:51:50 PMLast edited by: rh1990 at: 11/23/2017 1:52:24 PM |
|
This contribution was helpful to
3 thankful Users |
Follow us on