8/21/2017 10:51 AM | |
Joined: 10/3/2016 Last visit: 1/18/2023 Posts: 38 Rating:
|
How? I also have CU 305-PN version 4.40.45. Starter is V4.5.1.5 and SSP is V4.4 SP3 but my problem on the attachment is not solved. I am directly connected to S110's X150PN(LAN) with an ethernet cable. How can I change that default 0.0.0.0 IP and what should I do to connect? ------------------------------------------------------------------------------------------ |
Last edited by: The Troodon at: 8/21/2017 10:56:10 AMLast edited by: The Helping Hand at: 8/21/2017 2:30:57 PMNew subject after splitting |
|
8/21/2017 11:07 AM | |
Joined: 5/12/2006 Last visit: 1/27/2023 Posts: 21197 Rating:
|
hello, right click on the S110 in accessible nodes -< set IP |
8/21/2017 11:53 AM | |
Joined: 10/3/2016 Last visit: 1/18/2023 Posts: 38 Rating:
|
Solved. Thank you very very much. |
Follow us on