10/21/2022 2:54 PM | |
Joined: 8/31/2022 Last visit: 11/11/2022 Posts: 3 Rating: (0) |
I have a Modicion M340 Schneider PLC which is connected via an Ethernet cable to a local PC with monitor. On this PC I have TIA Portal V17 with a project consisting of only one SIMATIC WinCC Unified device. In this project I have connected it with the communication driver "Standard Modbus TCP/IP" and filled in the addresses of the PC and PLC. When I make a tag, I can connect it with the PLC. If I use address 4x400201 for example and use a tag on my PLC with the address %MW200 it works. But only one way... I can only write a value on the PLC-tag and that changes the value of my HMI-tag, but not the other way around. For some reason it also does not matter if I use the input or output register on the HMI tag (3x3 or 4x4). It remains an input. I think it has something to do with the function code which Modbus uses. I know that function code 23 is not possible (read/write register), but function code 3(Read consecutive integer values) and 6(Write single integer value) should be possible. So, I believe that it is somehow locked in function code 3 (input) when it communicates with the PLC. Does anyone have any idea how to change this? Do I have to tinker with the CSP of the Modbus for Unified? Maybe I'm completely wrong and if so please tell me. for the PLC, I'm using a BMX CPS 2010 with an Ethernet connection. And the project only uses 1 tag for now to test. Without any READ_VAR or other extra things, it still can access the tag of the HMI. the pictures are there for some clarification of the function codes I mentioned. Attachmentpictures of m340 and wincc unified modbus.zip (396 Downloads) |
10/28/2022 11:49 AM | |
Joined: 8/31/2022 Last visit: 11/11/2022 Posts: 3 Rating: (0) |
*The BMX CPS 2010 is a Power supply module. The PLC is I'm using is a BMX P34 2020. |
Follow us on