5/6/2016 1:50 PM | |
Joined: 3/28/2015 Last visit: 12/7/2023 Posts: 719 Rating:
|
Hello, 1-You need the original HMI program not a backup to be able to change the device type from KTP 600 to KTP 1000 and make the necessary modifications. 2-HMI Backup not editable and downloaded into the same type of panel. |
Eng.Mohamed Ibrahim |
|
5/6/2016 2:45 PM | |
Posts: 310 Rating:
|
Hello, Ya, I have Original Program File . So i want to convert to Ktp 600 to ktp 1000.. It is possible ..?? Thanks & Regards, Arasan.. |
5/7/2016 9:21 AM | |
Joined: 5/28/2008 Last visit: 12/5/2023 Posts: 4486 Rating:
|
Hello, Go to device settings in the left hand side navigator and select the new device (KTP1000). Then follow instructions here: Which settings should you make in WinCC (TIA Portal) prior to copying an HMI screen into another HMI operator panel? |
Ayman Elotaify |
|
This contribution was helpful to
3 thankful Users |
Follow us on