6/2/2023 5:41 PM | |
Joined: 7/19/2022 Last visit: 4/23/2025 Posts: 436 Rating:
|
Hello vladimir_3, I have also been testing it and I think that Unified is not possible with these functions. To know the status of the PLC what I do is send a bool from the PLC to the screen that remains for a second with the value at 1 and a second with the value 0, on the screen through scripting the change is checked Between 1 and 0, if the change does not occur, there is a problem with the PLC. |
If this Information really helps, you could use the Rate function |
|
Follow us on