12/30/2016 12:26 PM | |
Joined: 1/15/2015 Last visit: 3/22/2022 Posts: 66 Rating:
|
[snip] ... i have another question please. is it possible yo have more than one PG/PC interface?in my plant i have a wincc proj. and the communication btwn the CPU and the PC is being via cp343 thats why the PG/PC interface is set to the ethernet card.now if i want to go online to the CPU i am not able to access the CPU from the cp343(CPU is not accessible in the view accessible node) so i have to use the MPI/Profibus PC adapter and the PC adapter will not work until i change the set PG/PC interface to "PC adapter MPI or Profibus" and in this case the wincc proj. loses the communication with th CPU.So how can i make two PG/PC interface one ethernet for the Wincc proj.and another MPI for the PC adapter. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/31/2016 11:46:30 AMNew subject after splitting |
|
Follow us on