5/10/2019 7:00 AM | |
Joined: 9/12/2016 Last visit: 6/26/2022 Posts: 17 Rating:
|
dEAR vIPZ, i AM ALSO STUCK IN THIS PROBLEM.HOW CAN I UPDATE FIRMWARE IN THE STEP7 AND ALSO IN THE CONTROLLER. IN STEP7,I CANNOT FIND V4.3 FIRMWARE.PLEASE,HELP.DUE TO THIS,INITIALIZE PROXY NOT HAPPENING AND SHOWING SAME ERROR. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2019 11:38:54New subject after splitting |
|
5/10/2019 7:28 AM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
Hello, this device is to old. You must switch the HW to D445-1 or D445-2.
Christoph |
5/10/2019 8:11 AM | |
Joined: 9/12/2016 Last visit: 6/26/2022 Posts: 17 Rating:
|
PLEASE,FIND THE (IMAGE1) WHERE FW V4.3 CANNOT BE FOUND FOR D445 IN STEP7 HARDWARE. HERE,WE HAVE ONLY SUPPLIED KP700 TO OUR CLIENT AS WE NEED TO REPLACE EXISTING OP177B COMMUNICATING WITH D445 Control Unit; Firmware V4.1 - PN V2.2 with SINAMICS SM150 V2.6.2. I HAVE MIGRATED IN TIA PORTAL THE WINCC FLEX PROJECT,BUT TO BRING SIMOTION DRIVER,I NEED TO INITIALIZE DEVICE PROXY BUT INITIALIZATION IS NOT BEING DONE AFTER SELECTING .MCP FILE IN U7 FOLDER,BECAUSE D445-FW V 4.3 IS NOT AVALAIBLE IN STEP7 HARDWARE,DUE TO WHICH ERROR IS COMING(IMAGE 2). PLEASE,TELL HOW TO BRING D445 FW-V4.3 IN STEP7 HARDWARE. ORDER NO IS 6AU1 445-0AA00-0AA0,U CAN SEE IN (IMAGE1) AttachmentIMAGE1N2.pdf (545 Downloads) |
5/10/2019 8:19 AM | |
Joined: 9/12/2016 Last visit: 6/26/2022 Posts: 17 Rating:
|
PLEASE,FIND THE (IMAGE1) WHERE FW V4.3 CANNOT BE FOUND FOR D445 IN STEP7 HARDWARE. HERE,WE HAVE ONLY SUPPLIED KP700 TO OUR CLIENT AS WE NEED TO REPLACE EXISTING OP177B COMMUNICATING WITH D445 Control Unit; Firmware V4.1 - PN V2.2 with SINAMICS SM150 V2.6.2. I HAVE MIGRATED IN TIA PORTAL THE WINCC FLEX PROJECT,BUT TO BRING SIMOTION DRIVER,I NEED TO INITIALIZE DEVICE PROXY BUT INITIALIZATION IS NOT BEING DONE AFTER SELECTING .MCP FILE IN U7 FOLDER,BECAUSE D445-FW V 4.3 IS NOT AVALAIBLE IN STEP7 HARDWARE,DUE TO WHICH ERROR IS COMING(IMAGE 2). PLEASE,TELL HOW TO BRING D445 FW-V4.3 IN STEP7 HARDWARE. ORDER NO IS 6AU1 445-0AA00-0AA0,U CAN SEE IN (IMAGE1) AttachmentIMAGE1N2.pdf (581 Downloads) |
5/10/2019 8:25 AM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
hello, there exist no FW V4.3 for this device! you can not use FW V4.3 with this device! regards |
5/10/2019 8:26 AM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
hello, there exist no FW V4.3 for this device! you can not use FW V4.3 with this device! regards |
Follow us on