9/8/2019 12:48 AM | |
Joined: 11/12/2015 Last visit: 12/30/2024 Posts: 13 Rating:
|
Hi Duris, Maybe it is very long time ago but I have a problem at same subject. But I want to use only reiceve command, is it possible to use receive command as this document. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/09/2019 13:00:03New subject after splitting |
|
9/9/2019 11:19 AM | |
Joined: 11/12/2015 Last visit: 12/30/2024 Posts: 13 Rating:
|
Hi Durris Firstly I'm new at Simens plc programing, and 2 years ago I write this program. I remember that it was running and I can get the card id, but now it is not running. I use S7 1500 plc, and Cm Ptp Rs422/485 BA. I connect a card reader to with 2 wire 15 pin socket. I need only get to card id, normally it has 8 caracter in hex. But now I counldnt get it. How can I receive the data reading by RS485. Is it true to use Receive config, and what about the the inputs. Please find the picture about config also. Thanks for help. Best Regards Harun Attachmentpicture.zip (178 Downloads) |
9/10/2019 8:33 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
You're welcome, glad you have a success... |
With best regards... |
|
Follow us on