6/29/2023 9:09 AM | |
Joined: 10/20/2016 Last visit: 8/2/2023 Posts: 11 Rating:
|
Wie kann ich mir den Status einer 1508SF anzeigen lassen? How can i see the status of a SoftPLC 1508SF? ------------------------------------------------------------------------------------------ edit: Thomas |
Last edited by: Jen_Moderator at: 06/29/2023 12:36:43New subject after splitting Last edited by: Supergrobi70 at: 06/29/2023 15:18:57 |
|
6/30/2023 6:21 AM | |
Joined: 1/21/2013 Last visit: 9/29/2023 Posts: 2084 Rating:
|
Hi Thomas, You should describe your problem in more detail. What version of WinCC Unified are you using? Are you using a Unified Comfort Panel or WinCC Unified PC Runtime? In case of PC Runtime, is it installed on the same PC as the CPU1508S F? What do you mean by "But if i drag this object to my screen nothing happens."? Do you mean that you do not see the expected object in the engineering or does this only affect the loaded runtime? But to be honest, what you describe sounds like a bug to me. So if you have already installed V18 with all available updates, you should contact Siemens and create a support request. Kind regards |
This contribution was helpful to
1 thankful Users |
6/30/2023 6:38 AM | |
Joined: 6/19/2017 Last visit: 9/29/2023 Posts: 7329 Rating:
|
Thank you for editing your post and making your question more understandable! Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to
2 thankful Users |
7/4/2023 12:27 PM | |
Joined: 10/20/2016 Last visit: 8/2/2023 Posts: 11 Rating:
|
hi Forum,
The 1508 is a own Device on an own IPC the HMI Software Version (Unified RT) was actual V18 Update1 SR1 at this time and is installed on a other PC (only for the HMI).
with this i mean i drag the diagnostics object to a Screen an start the Runtime, but on the RT screen i have only a window with nothing inside. On my HMI i get tags, values, grafics, buttons an more, but this system diagnostic doesnt work with a SoftPLC. So i will open another SR... Thanks anyway |
Follow us on