7/23/2018 11:09 AM | |
Posts: 1283 Rating:
|
Hi Duris, How can i send define the TSEND data as Hexadecimal. In the Hercules software there is option to use Hex characters to send. Only when i define that the Power meter send back data. if i don't enable hex the power meter doesn't respond. Am i doing something wrong in the DB side in assigning the data types? I used Struct data type and then defined the send parameters like how Milos defined in his program. Not sure whether it is right for me. Also another question, is it possible to check using Telnet cmd like how the Hercules software does? Thanks, Jay ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/24/2018 10:38:42 AMNew subject after splitting |
|
7/24/2018 8:12 AM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
You're welcome Jay... |
With best regards... |
|
Follow us on