1/13/2016 7:40 PM | |
Posts: 19 Rating: (1) |
We are using an OPC ua for HMI connected to Old PLC S5. Read / write to PLC is working for configured DB's on screens. My question is how can we use the PLC Status/Force control in HMI to show/change user variable I/O, DB? When the screen that has status/force control is displayed, there are no connections that appear in drop-down. The connection is setup as OPC UA ------------------------------------------------------------------------------------------ Attachmentplc_status_force.zip (304 Downloads) |
Last edited by: Min_Moderator at: 1/15/2016 10:38:08 AMNew subject after splitting |
|
Follow us on