12/13/2012 9:55 AM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
Tks I did it many time - graphics not changed! How u change language in RT?
|
12/13/2012 1:21 PM | |
Posts: 8946 Rating: (999) |
Andy, please doublecheck, if you really select the desired language at the runtime setting, see attached picture. |
12/13/2012 3:11 PM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
Yes - all the same Language - CHANGED (no problem) Graphics DONT change
|
12/13/2012 3:46 PM | |
Posts: 8946 Rating: (999) |
I advice you to upload your program. Find also a small example attached, it is working fine. AttachmentE:\RT_Language.zip (116 Downloads) |
This contribution was helpful to1 thankful Users |
5/27/2015 9:20 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640) |
Hello everybody I Think it wont work automatically in WinCC Professional like in a Advanced Runtime. I added a Professional Runtime in the sample Project of this thread. You can work with a Grafic List and set an internal Tag with the LCID of you Language. so set your Internal Tag with your current LCID and the Picture Change will work with a symbolic Graphic field. You have to set the Change of your Grafic in case of Language change by yourself. I the sample it works fine. I hope it helps you. Bye Moruf ---------------- If this Information helps you could use the Rate Button AttachmentLanguage_V13_SP1_GL.zip (131 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on