4/21/2022 1:33 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12867 Rating: (1639) |
Hello SpeedsterJuss what do you mean with JS-> Javascript?? if yes then you are in the wrong conference. WinCC V7 can only use VB SCript and CScript (and VBA but only in engineering in Graphics designer). Are you using WinCC V7.X or are you using WinCC Unified? It is important because the way of programming are very different... (if you are using WinCC Unified then have a look at https://support.industry.siemens.com/cs/ww/en/view/24325381 chapter 5.4 in the documentation) |
If this Information really helps, you could use the Rate function |
|
4/5/2023 12:18 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12867 Rating: (1639)
|
Hello SpeedsterJuss Here you find also detailed description to your topic and also to scripting in general: https://support.industry.siemens.com/cs/de/en/view/109758536 ( for example Chapter 5.4.5) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on