7/3/2020 9:30 PM | |
Joined: 8/23/2019 Last visit: 8/29/2024 Posts: 58 Rating: (0) |
Hallo all, In my application using Sinamics drive V90 and Simotics motor for Flying Saw & Punch Machine. Commissioning Flying Punch & Cutting Machine I used PLC S7 1214 as main controller is connected by profinet to Sinamics drive V90. My problem is how to keep down of winding temperature on Motor while running 30 minutes. I ever try to run it until 1 hour then monitoring by V-Assistant recorded winding temperature about 100 degree Celsius. Please help me how to solve my problem. The machine will running automatically until 6 hour/ day without never stop. I am afraid much that it will make Sinamics drive & Simotics motor will be broken soon. Thanks so much Sahala |
Follow us on