8/31/2018 11:18 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Please see attached screenshots. I would like to know which tag / signal that makes my little square go from grey to green. With other elements with dynamic properties I can double click on the little lightning under dynamic but with these little squares that action only deletes the lightning (so that the tag is no longer dynamic on that property) Not only is the dynamic property deleted the Grapics Designer is frozen and this application as well as the WinCC Explorer must be closed with the Windows Task Manager. Why is that happening and what is the correct way to find the tag? AttachmentWCC.zip (86 Downloads) |
Last edited by: xmnj at: 8/31/2018 12:37:36 PM |
|
9/3/2018 8:48 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hi Georg, That sounds good :-) But then I am reading your link completely wrong (on how to create a memory dump - but how do I do it WITHOUT installing additional software (and what can I see in the memory dump)?: "How do you create a memory dump for diagnostics purposes in WinCC and PCS 7?
The instructions below are for installing and using a memory dump in WinCC and PCS 7. You can use this tool to create a memory dump of a process in the event of a fault. This memory dump can be useful for detailed diagnostics. Procedure for Windows 7 and higher (Windows 7, Windows 8.1, Windows Server 2008, Windows Server 2008 R2 and Windows Server 2012 R2, Windows 10)Procedure for Windows 2000/2003 Server/XP Procedure for Windows 7 and higher (Windows 7, Windows 8.1, Windows Server 2008, Windows Server 2008 R2 and Windows Server 2012 R2, Windows 10)Contents
|
Last edited by: xmnj at: 9/3/2018 8:49:07 AM |
|