5/23/2017 9:24 AM | |
Joined: 9/30/2016 Last visit: 6/4/2025 Posts: 941 Rating:
|
I have a PLC I use to test the SW and I need to test SW for different plants (with different IP addresses). So it is running with old SW from a old project and I want to DL SW from a new projekt. It seems to go well - except that the IP address is not updated. See also the attached screenshot. I have tried to delete the HMI connecttion and redraw it and download again - but still no success. How do I get the right IP address into the controller - so I get connection to my tags ? I have previously had a similar problem which was solved with help from here. |
5/23/2017 1:32 PM | |
Joined: 9/30/2016 Last visit: 6/4/2025 Posts: 941 Rating:
|
Hi again ChristophD, I am not really sure how - but I succeeded in getting the IP address set to .11 so that is nice. But for some reason I cannot get the HMI panel connected to the project. Please see attached screenshots. It is red when online and I tried deleting it and reconnecting it - but it changes nothing. How do I make a correct and functioning connection between the PLC and the HMI panel (.IP addresses .11 and .14) ? AttachmentConnection to HMI panel.zip (306 Downloads) |
5/23/2017 3:38 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4763 Rating:
|
|
Follow us on