5/11/2017 10:48 AM | |
Joined: 9/30/2016 Last visit: 4/24/2025 Posts: 938 Rating:
|
With some help I have made a small project in a S7-1500 PLC with both WinCC classic and TIA WinCC Advanced operator interface (CCR & local Comfort panel). I have added a new setpoint to the PLC for the operator to be able to type in a value / setpoint. I need to put a faceplate and pop-up for this signal - but I cannot pick it in the pull-down menu. I am guessing that this is because the signal is not in the HMI tag list. I am pretty sure I did not add all the PLC signals til the HMI list manually - but how do I get my new signal into the HMI system so I CAN pick it. See also attached screenshots. AttachmentTags to HMI.zip (75 Downloads) |
5/15/2017 8:35 AM | |
Joined: 9/30/2016 Last visit: 4/24/2025 Posts: 938 Rating:
|
Are there really no one at all that can help with this ? |
5/15/2017 11:51 AM | |
Posts: 648 Rating:
|
Are you really sure? Did you check the number of chars? In your screenshot your tagsname is false. With best regards rh1990 |
Follow us on