8/20/2018 11:04 AM | |
Joined: 9/30/2016 Last visit: 4/24/2025 Posts: 938 Rating:
|
Please also see the screenshots. I am adding a new display to a 7" flex panel. I can add the display and make the buttons (both sets) working correctly but the text on the "virtual button is only shown when the screen is active. I have compared with the other buttons (which are working correctly) but I cannot spot what I am missing? AttachmentTræk 1AB.zip (33 Downloads) |
Follow us on