10/10/2016 9:24 AM | |
Joined: 9/30/2016 Last visit: 4/24/2025 Posts: 938 Rating:
|
I am struggling to install WinCC Comfort Advanced V13.0 SP1 on my work laptop (any expert please verify that this IS the version my project is telling me I need). I AM a local administrator and I do the restart the installation package requires but after the PC is restarted and the installation should start is just ask for another restart - how can I get past this "self-lock"? I have the same issue with the Simatic S7 PLCSIM v13 installation. For references please see attached file (how do I attach multiple jpg images to a post ?) AttachmentScreenshots 2.pdf (190 Downloads) |
10/10/2016 9:30 AM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
have yxou check the steps in this FAQ? https://support.industry.siemens.com/cs/ww/en/view/8861819 Regards Christoph |
This contribution was helpful to
1 thankful Users |
Follow us on