5/23/2017 2:39 PM | |
Joined: 9/30/2016 Last visit: 6/4/2025 Posts: 941 Rating:
|
I had some troubles getting the IP address in the project into the PLC - but I finally succeeded in getting the IP address set to .11 so that is nice. But for some reason I cannot get the HMI panel connected to the project. Please see attached screenshots. The connection is red when online and I tried deleting it and reconnecting it - but it changes nothing. How do I make a correct and functioning connection between the PLC and the HMI panel (.IP addresses .11 and .14) ? AttachmentConnection to HMI panel.zip (1156 Downloads) |
5/23/2017 3:03 PM | |
Posts: 8946 Rating:
|
There is no need to use "Topology" window if you are not running Isochron - mode. |
5/24/2017 8:20 AM | |
Joined: 9/30/2016 Last visit: 6/4/2025 Posts: 941 Rating:
|
Hi again, I have not (intentionally) used portinterconnection - but how do I check if it IS used ? The panel IS connected via profinet with its own IP address. (See offline screenshot) I don't THINK the panel is configured as an I/O device (how/where do I check that ?) but the system can be operated from it - including setting analog signals to a manual value - from the panel. Even though the small plant CAN be controlled for the local panel it is supposed to be monitored and controlles with many other systems from a CCR. Right now I don't have a physical panel. I am using the simulation function in TIA to verify the functionality of the PLC code. I guess I can see the IP A of the physical panel by searching for compatible devices with the "go online" function in TIA - but how do I check the name (to be the same as in the project) AS I am simulating the panel right oicking the wrong port on the panel is not likely to be causing my problems - but I will try to remember when I move to the actual plant. (See offline screenshot) I am TOO well aware that this is basic but HOW/WHERE do I find the diagnostic messages for the panel to see if "Wrong Partner port" or similar is listed - is it when I go online ? (See offline screenshot)
AttachmentIP Addresses & connections.zip (615 Downloads) |
Follow us on