7/24/2018 9:13 AM | |
Joined: 9/30/2016 Last visit: 4/28/2025 Posts: 938 Rating:
|
Please also see attached screenshots. I need to make a visualization of positions of some gear levers on a KPT700 Basic Flexpanel. The visualization has already been made in WinCC 7.4 SCADA and it has to look similar on the flexpanel. In WinCC 7.4 SCADA the levers have been drawn as lines with a really big circular end but I cannot find this linetype in the basic WInCC so I have drawn the levers with a line and a circle. I have grouped the 2 elements for each lever in order to be able to treat them as one element. I need the lever to change between black (when the lever is in that position) and (background) grey (when it is not). But I cannot find the option for dynamic color change for the grouped element - only the to components? Attachmentgz.zip (251 Downloads) |
Follow us on