1/9/2020 11:17 AM | |
Joined: 10/3/2010 Last visit: 7/5/2024 Posts: 1556 Rating:
|
Please make sure that the "Global color scheme" attribute of your object is set to "No"! (Object Properties -> Effects -> Global Color Scheme) |
B r g d s , |
|
1/13/2020 8:07 PM | |
Joined: 3/14/2018 Last visit: 6/20/2024 Posts: 32 Rating:
|
I have found a workaround. Not what i was expecting but it should would work as i want. I needed to apply changes in background RGB color and transparency. It appears setting transparency would not work so i tried to set the profiles in global color palette. As it wasn't possible to use them inside faceplate i went to the ultimate solution. I used the example here: https://support.industry.siemens.com/cs/tw/en/view/11842395 Then i made some modifications so it could output the color code wich is the RGB color multiplied by the transparency factor wich gives a number. With this number, comes the RGB color and the transparency together, so instead of referencing to the collor palette color index, i just reference the color number and then the color + transparency works well. |
Last edited by: Jen_Moderator at: 01/14/2020 10:06:40Optimized link. |
|
Follow us on