2/9/2023 1:16 PM | |
Joined: 3/11/2019 Last visit: 3/20/2023 Posts: 713 Rating:
|
Hi xmnj, in this case, this message can be ingored as firmware V4.5 is backwards compatible down to V4.0 Release S7-1200 CPU Firmware version V4.5"To configure the SIMATIC S7-1200 CPUs version 4.5 and higher it requires the Engineering System Step7 with version V17.0 and higher" "An S7-1200 CPU with version 4.5 is replacement compatible with an S7-1200 and firmware version 4.0, 4.1, 4.2, 4.3 and 4.4. This enables the use of a real existing CPU with firmware version 4.5 with an engineered V4.0, V4.1, V4.2, V4.3 or V4.4 based on an existing TIA portal older versions project." regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
2 thankful Users |
Follow us on