3/19/2016 12:19 PM | |
Joined: 3/5/2013 Last visit: 11/5/2024 Posts: 19 Rating: (1) |
When I try to choose the variables to trend, the window comes out all grey and there is no possibility to push anything |
3/21/2016 9:39 AM | |
Joined: 8/3/2009 Last visit: 1/16/2025 Posts: 14583 Rating: (1815)
|
Hello mrvoice Yes this is a normal behaviour. You have to do what K!ke has written in the Post above! Drag the property Trends to the Intervaces in the middle Screen. I Have made a Screenshot where you can see. The Trens you can only set outsinde the Faceplate an the Interface of the Faceplate instance. Bye Murof Attachmentfaceplatetrend.zip (1096 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to3 thankful Users |
4/13/2016 11:06 AM | |
Joined: 8/21/2014 Last visit: 1/16/2025 Posts: 1036 Rating: (14) |
New question published by ziemson is split to a separate thread with the subject Adding more than one trend on the faceplate. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on