11/22/2015 6:12 PM | |
Joined: 2/20/2007 Last visit: 11/19/2024 Posts: 122 Rating: (2) |
Dear All,
I have installed PCS7 V8.1SP1 in my plant. Still OS client is requesting through wincc license analysis WINCC RC and RT licenses. Although I have installed PCS7 V8.1 OS Client license in ALM. When I am checking OS Client license , it is coming OK. OS Servers are working fine with PCS7 Server and OS RT PO license. Can anyone explain , how I can change the settings of ALM so that it can use PCS7 OS Client License instead of giving error for WINCC RT License.
Regards,
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/23/2015 3:53:43 PMNew subject after splitting |
|
Follow us on