6/2/2012 9:11 AM | |
Posts: 8946 Rating: (999) |
Bad luck, you can not remove it. Also I do not know any "illegal" tool to do it. |
6/2/2012 12:09 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, is the plc write-protected or read/write-protected? You have the offline-program? If the plc is only write-protected then you can compare the program. It is possible to the remove the password in the hardware config and transfer the program to a not protected MMC-card. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
6/11/2012 4:03 PM | |
Posts: 41 Rating: (1) |
Is there an illegal way? Just asking? |
Follow us on