3/19/2018 11:56 AM | |
Joined: 4/29/2010 Last visit: 2/7/2025 Posts: 19 Rating:
|
Hi I'm using MC_gearinpos with 1515T and tia portal 14 SP1. How is possible to configure the block to execute the movement of the slave axis to the master position before start the master? Is my first machine with technology cpu S7 1500, i use simotion D and the function MC_gearin or "Enablegearing" already have this possibility, to synchronize the slave while the master is stil, and after this movement the slave is in gearing and the master is ready to start? How is possible to make this also with _mc_gearinpos? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/20/2018 11:10:14 AMNew subject after splitting |
|
3/19/2018 2:42 PM | |
Joined: 4/28/2015 Last visit: 10/25/2024 Posts: 398 Rating:
|
Hello, did you see the application example... https://support.industry.siemens.com/cs/de/en/view/109744840 Maybe you will find some information about functionality in the basic example... |
Follow us on